This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS254900A-Q1: Schematic review

Part Number: TPS254900A-Q1

Tool/software:

Hi Teams,

Please help to review TPS254900AIRVCRQ1 schematic, thanks.

  • Hi Che,

    Please find the following comments:

    1. increase the voltage rating of C381, to avoid the capacitance drop when voltage applied close to abs value. >16V rated cap suggested.

    2.Missing wires for DM_out and DM_in.

    3. CTL1/CTL2/OVP thresholds can be find in section 6.5 in the datasheet, please design the resistor divider's accordingly (for example R1&R5). 

    4. Please check if the voltage rating of D9 is too low for your application.

    Thank you.

    BR,

    Ke Wang