This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: PMID drop off on unplugging causes CM5 to shutdown

Part Number: BQ25895
Other Parts Discussed in Thread: BQ25638, TPS61088

Tool/software:

Hi!

Ive designed a custom CM5 carrier board and it seems to work well except on unplugging VBUS power in the Pi which is powered via 5V PMID shuts down. I think this is due to a short drop off as it switches to battery but is there a simple way to fix this issue? I was thinking of adding more capacitance on the PMID pin or maybe a super capacitor but im not sure what the consequences of that will otherwise be. There isnt really board space otherwise to power via an external boost converter from the SYS output so I'm stuck in that regard.

Any help would be appreciated!

Kind regards,

Muhammad