This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A45: Efficiency of TPS7A4533

Part Number: TPS7A45


Tool/software:

Hello TI expert, I am interested in using TPS7A4533 to convert 5V to 3.3V. I am wondering what the efficiency of the LDO will be when load current is 600mA maximum and 200mA minimum. Do you have an efficiency curve for this part that you can share?

Thanks,

Joe 

  • Hi Joe,

    The efficiency for any LDO = Output Power / Input power = (Vout x Iout)/ (Vin x Iin)

    Since Iout = Iin for an LDO, for your specific use case, the upper bound on the efficiency of the TPS7A4533 = 3.3/5 = 66%

    I say upper bound because the actual efficiency will be slightly lower. The Iin will include quiescent current as well i.e. Iin = Iout + Iq

    Regards

    Ishaan