Tool/software:
Designing a PD Source.
Prefer 240W with PPS/AVS.
I found TPS26744 which seems to be exactly what I need.
I want a PD source controller that can control a DC/DC converter, with no MCU.
So a few questions:
- When will TPS26744 be on the market? Can I order preproduction? When?
- When will EVM be available?
- Are there any similar chips o the market, i.e. USB Source controller that controls a DC/DC? Does not have to be automotive, can be single port, USB only. Prefer 240W/PPS/AVS, but other EPR options can be accepted. Input voltage is not specified.
- Is there any programming involved or is it plug and play? I understand there is a GUI. How are settings uploaded without MCU/external EEPROM?
Thanks.