Tool/software:
Hello all,
I have configured the BQ25895 to use the ILIM pin to set my input current limit to 1.5A. IINLIM is set to 3.25A. D+ and D- are shorted in my implementation since I do not need USB compatibility.
If I have ICO disabled my understanding is that the actual input current limit will be the lower value between the ILIM pin and IINLIM register value. So in this case it is 1.5A. If ICO is enabled my understanding is that the actual input current limit will be the lower value between ILIM pin and IDPM_LIM register value NOT IINLIM. Is this understanding correct?