This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659037: TPS659037

Part Number: TPS659037


Tool/software:

We have selected this PMIC IC part number, but we need to ensure it meets the requirements outlined below. Kindly review the specifications and confirm whether the selected part meets all the specification listed below. And also please let me know any other part which meets out requirement criteria.



minimum voltage should be 0V

Step size / resolution : 1mV

Current rating <2A

Ripple voltage : 1mVrms

Volt meter resolution : 100 uV

Ammeter : 10uA

  • Hi Mohankumar,

      The PN TPS659037 you're checking is our legacy part now; it was designed >12 years ago. We no longer support the device for any new design.

      Also, we have no any power device can meet your required criteria.

    Thanks!

    Phil