This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5113: LM5113QDPRRQ1

Part Number: LM5113


Tool/software:

lm5113pcb.pdf

This is the schematic diagram of the LM5113 I used. When I apply HIGH to the HI pin and LOW to the LI pin (with HIGH = 3.3 V in my case), the HS pin only rises up to 2.56 V. Then, when I set HI = 0 and LI = 1, the HS pin goes to 0 V, which works correctly. But in the first condition, it doesn’t work, and my phase output stays at 2.56 V instead of 5 V. Can anyone help me debug this issue? I have already tried removing the zener at the OL pins and changing the gate resistor from 340 Ω to 10 Ω, but the issue remains.