Tool/software:
Hello there,
At the moment we are testing our hardware. During these tests we found out that the battery current meassured a value of 0mA during discharge of the battery, during charging everything seems fine. All the other ADC channels are reading out fine during discharge. So what are we doing wrong? We almost use the same circuits as shown in the datasheet (our load is connected to the high side of the battery shunt resistor and we removed BATFET [Q3,Q4] as they were optional), we expected to measure the current discharging the battery this way, as the internals switch the internal power automaticly between VAC and SRN. The ADC is enabled and running in continous mode, the IBAT channel is enabled just like all the other channels. Is there something we are missing? Could you please help us to figure out why this function isn't working?

Kind regards,
Teun