This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS628301: How to select inductors for TPS628301

Part Number: TPS628301


Tool/software:

I have a question regarding the inductor selection for the TPS628301.

According to the datasheet, the following information is given about the inductor:

  • Recommended Inductor: 0.24 to 1 µH (from section 6.3 Recommended Operating Conditions)

  • Inductor Calculation Formula: shown in the figure in section 8.2.2.3 Inductor Selection

For my application, the conditions are:

  • IOUT,MAX = 300 mA

  • ΔIL = 90 mA (IOUT,MAX × 30%)

  • fSW = 2 MHz (fixed)

  • VIN = 5 V

  • VOUT = 1.8 V

Based on these conditions, the calculated inductance value is about 6.4 µH.
However, section 6.3 (Recommended Operating Conditions) specifies a maximum of 1 µH, which is a large discrepancy compared to the theoretical value.

My questions:

  1. Is it acceptable to select an inductor greater than 1 µH (e.g., 6.4 µH) in this case?

  2. If I choose 1 µH, considering inductor tolerance (e.g., ±20%), the actual value may exceed 1 µH. Should I understand the “MAX 1 µH” in section 6.3 as excluding tolerance?