Tool/software:
I have a LM25576 Inverting Buck-Boost circuit. Vin =+14.5 - 15.5V. Vout = -15V. Iout = 1.5V. The design was copied from Webench simulation.
All 5 prototype boards only generate -15V at 1.1A maximum. At 1.5A, the output voltage is approximately -12.5V.
Could you please suggest which components should I investigate or adjust to improve the output current?
Thanks,
Jason