UCC256404: Full-Bridge LLC with UCC Controllers and Three-Phase LLC Solutions

Guru 12155 points
Part Number: UCC256404
Other Parts Discussed in Thread: PMP

Tool/software:

Hi Support Team,

I would like to ask about control methods for LLC resonant converters, specifically in the following two areas:

  1. Full-bridge LLC control using analog ICs
    As I understand, the UCC series (e.g., UCC2564xx, UCC25630x, UCC25661x) is mainly designed for half-bridge LLC applications.
    Is there a recommended way to implement a full-bridge LLC using these controllers?
    If so, could you please suggest the most suitable ICs and provide any available reference designs?

  2. Three-phase LLC control
    Is there any method to control a three-phase LLC resonant converter with a single IC?
    If this is not feasible with analog ICs, I assume digital control (e.g., using a C2000 MCU) would be the practical approach. Could you recommend the appropriate devices and any reference designs or application notes (such as PMP/TIDA examples)?

Thank you very much for your support.

Conor

  • Hi Conor,

    1. Full bridge LLC can be developed by UCC25661x and using isolated gate gate driver UCC5350SBDR. 

    There is no reference design still published. But the circuit will be like below figure:

    Where HO1, HO is connected with HO pin of UCC25661x; and HO is connected with HO pin of UCC25661x

    2. Three phase LLC is not possible by analog controllers. You can create a new thread in C2000 to check the feasibility. 

    Regards,

    Sougata

  • Hi Sougata,

    ■ Additional question to question 1
    Thank you for the reference circuit diagram information. Are there any plans to release a reference design for the UCC25661x + UCC5350SBDR combination? If so, please let me know the specific release schedule.

    ■ Comment on question 2
    I understand that this cannot be achieved with an analog IC.
    I will repost this on the C2000 forum!

    Thanks,

    Conor

  • Hi,

    I will check internally if we have any plan to release this type of reference design and get back to you as earliest as possible

    Regards,

    Sougata

  • Hi Sougata,

    Do you have any update?

    Thanks,

    Conor

  • Hi, Conor,

    We do not have any plan to release this type of reference design in recent days. Will update you if something got decided. 

    Regards,

    Sougata