Other Parts Discussed in Thread: TPSM83102
Tool/software:
Tool/software:
Hi Dattaguru,
It's really strange.
For the schematic, MLCC caps for Vin and Vout is suggested. No other concerns.
For the layout, it needs to be optimized, you may refer to the layout example in the datasheet.
Well, all these factors should not make the device no output. Please have a quick measurement on the Vin and EN (as close as to the chip).
Regards
Lei
Hi Lei Zhong
Hi Dattaguru,
Please ignore my previous comments about the MLCC caps. I thought only electrolytic caps are used since the symbol in the schematic. So the schematic is OK.
Have you measured the real Vin and EN voltage on the node that as close as to the chip? And please also double check the feedback resistors R4 and R11.
And if the module device was mounted manually on board by hand, please check whether the inductor is still well mounted on the module substrate.
If the real voltage on the VIN and EN pin are both 5V, the feedback resistors are correct, and the inductor is still well connected, the module device should work normally.
Regards
Lei
Hi Lei Zhong,
Have you measured the real Vin and EN voltage on the node that as close as to the chip? And please also double check the feedback resistors R4 and R11.
Ans: Yes. Voltage on Vin ane EN is 5V. R4 and R11 are 551K and 91K respectively
And if the module device was mounted manually on board by hand, please check whether the inductor is still well mounted on the module substrate.
Ans: The inductor [ black plastic package] is well mounted on the module substrate.
If the real voltage on the VIN and EN pin are both 5V, the feedback resistors are correct, and the inductor is still well connected, the module device should work normally.
Ans: VIN and EN are 5V
However, we are not receiving any output power when the board is operational.
Hi Dattaguru,
Could you help a quick check that whether the used chip is TPSM83100, not TPSM83102?
Regards
Lei
Hi Dattaguru,
One more trying, please use another fresh TPSM83100 unit.
And also double check whether the feedback resistors are correctly mounted.
Regards
Lei