Other Parts Discussed in Thread: LM5122
Tool/software:
Hello,
I am an FAE at a distributor that handles TI products.
My customer is considering a circuit with the following specifications.
This circuit requires a peak of 600W, but can the LM5156H meet this specification?
Also, is it possible to connect multiple LM5156H devices in parallel and operate them?
If yes, please provide any useful connection examples.
The reason we are considering this device is that we were initially considering the LM5122 synchronous rectification controller, but because the SW pin has a rated voltage rating of 105V, we are considering a different circuit configuration.
(Specifications)
VIN: 16V to 60V
VOUT: 100V
IOUT: 3A (steady state), 6A (peak, 5 seconds continuous)
Non-isolated
Best regards,