Other Parts Discussed in Thread: WEBENCH-CIRCUIT-DESIGNER, LM5177, UCC28C42
Tool/software:
Hello,
I am considering the following specifications.
When I checked your website using WEBENCH-CIRCUIT-DESIGNER, I was suggested to configure a circuit using the UCC28950.
I certainly think that the UCC28950 is an effective option for an isolated circuit.
However, I would like your opinion on whether my specifications can be achieved using a non-isolated IC such as the LM5177.
I would like to consider a simpler way to configure it.
(Specifications)
VIN: 16VDC to 60VDC
VOUT: 48V
IOUT: 6.5A (steady state), 9.5A (peak for 5 seconds)
Isolation required
Best regards,