Tool/software:
Can this converter (TPS552892) be used in an application where the input voltage is either 12 V or 24 V and the load current is 7 A at 12 V output?
Hi Sayan,
Thanks for reaching out.
May I know the application here?
The thermal would be a concern here. Recommend to select two pcs TPS552892 or use TPS552882 instead.
BRs,
Bryce