Tool/software:
Hello. I o design new power system from battery with webench help. I create prototype board. Design from webench is included. Output is regulated well with low load (0.1A), but increasing load not starts output pulses in OUTE and OUTF pins. Then output FETs not switching, only internal FETs diodes rectify output.
webench_ucc28950_design_forum.pdf
Here are outputs of Vout (yellow), Gate Mosfet E (blue), Gate mosfet F (green) and transformer output connected to Drain mosfet F. Output OUTE and OUTF not starts to switching.

The same output as OUTE and OUTF is in CS pin.
When I try to calculate values with https://dr-download.ti.com/design-tools-simulation/calculation-tool/MD-rlvLC7vkDZ/01.00.00.0E/SLUC222E.xlsx I got other values for some resistors. But there is big different between webench and SLUC222E - dividers ADEL and ADELEF are connected to CS pin (in webench and datasheet) but in SLUCC222E is connected to VREF. What is correct? I think here is any problem, why outputs E and F are not switched.