This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS923650: Dimming Issue

Part Number: TPS923650


Tool/software:

Hi

I have 3 questions regarding the TPS923650D2. It is being used in Boost mode to drive a string of LEDs and this is working fine.

1) Can the VCC pin (5v) be used in a resistor divider (resistor divider between VCC and ground) to supply the analog voltage to the DIM pin ?

2) At present im supplying the DIM pin voltage via a DAC and even though i have a small diode between the DAC and the DIM pin, the DIM pin voltage is already 6v. Is this ok ?

3) The VCC pin is 3.3V instead of 5V. Is this expected ?

Thank you for your inputs