Other Parts Discussed in Thread: TPS2378, TPS23731
Tool/software:
Hi
Could you help recommend a product that can replace the LT4275B.
Thank you.
https://www.analog.com/media/en/technical-documentation/data-sheets/4275f.pdf
Tool/software:
Hi
Could you help recommend a product that can replace the LT4275B.
Thank you.
https://www.analog.com/media/en/technical-documentation/data-sheets/4275f.pdf
Hello Gareth,
The closest replacement to the LT4275B would be the TPS2378, which is IEEE802.3at compliant (up to 30 W). Additionally, the TPS23731 is also IEEE802.3at/bt compliant with an integrated DC/DC CTL solution. Both datasheets are linked below.
TPS2378: TPS2378 IEEE 802.3at PoE High-Power PD Interface datasheet (Rev. C)
TPS23731: TPS23731 IEEE 802.3bt Type 3 Class 1-4 PoE PD with No-Opto Flyback DC-DC Controller datasheet
Best,
Anagha