This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1210-Q1: B2B FET Controller for BMS

Part Number: TPS1210-Q1


Tool/software:

Hello team,

My customer wants to use TPS12100-Q1 for 12V BMS, here are several questions:

1. Can it support bidirectional current? In the BMS, both discharge and charging are needed. Is there a logical conflict regarding reverse current operation (discharge) and reverse polarity protection?

2. Is there UV/OV monitoring for the input, output, and common source terminals?

3. How about the comparison with discrete solutions, such as functionality, performance, and cost, etc.

Thanks!

Regards,

Daniel