Other Parts Discussed in Thread: BQSTUDIO,
Tool/software:
Hi Team,
i am testing BQ25887EVM with BQSTUDIO. With 5V input, i set ADC at continuous mode with15b sample rate, then i enable ADC, the bqstudio can read both VBUS and VBAT correctly. if i remove VBUS and connect a 7v battery to EVM battery connector. the BQSTUDIO can communicate with the EVM, but i can't enable ADC( set 0x15 bit7 to 1, while read value is 0), could you please help check this and advise is there anything else i can do?
Regards,
Stone