TPS7H3301-SP: Power Output

Part Number: TPS7H3301-SP

Tool/software:

Hello, DS is a little confusing.  What is the worst case output current or max output current capability of the part assuming a VDD of 2.5V and VLDO of 1.2V.  Also, can we get a curve like that of Figure 6-13 for a DDR4 part with the input voltages I've specified?

We plan to use this part with DDR4 part: DDR4T08G72MZR2C-N1

Thanks,

  • Hi Joseph,

    This part is designed to nominally sink and source up to 3A. Figure 6-13 is meant to give an idea of how load regulation and current limiting would influence the output voltage, and how temperature can influence where the current limit may kick in.

    I don't know that we have additional data for the exact voltage configuration you're interested in, but I will look into it. Please give me a day or 2 to update on this.

    Thanks,

    Sarah