Tool/software:
I need to program these registers : 02, 20, 21, 24, 27, 29, 2B, 41, 45, 60, 61, 62, 63, 64, 65, D4, D5, D6, D7. I am using BPM programmer. Currently these registers are giving me NACK. I see in datasheet, something about PWOM_loop slave device. Can you please ellaborately explain on this. Also, I read the register 0x80. The data I get is 0x03. That means is_slave and sync_fit bit is set. Please let me know how to program those registers. Thanks!