Other Parts Discussed in Thread: TL431
Tool/software:
Good morning, everyone.
I need to build a non-isolated AC-DC converter with the following characteristics:
Input voltage: 240 VAC
Variable output voltage: V1 = 110 VDC, V2 = 60 VDC
Output current: 1 A
Do you have a controller in your catalogue that would be suitable for my needs?
Best regards,
Gianluca
P.S.
The part number is incorrect because I didn't know which one to use.