Tool/software:
We only have a 3.3 V supply available and would prefer not to generate a 5.5 V supply for the REGIN pin of the BQ76952.
Our MCU runs at 3.3 V and communicates with the BQ76952 via SPI. According to the datasheet (section 7.6), the SPI output high level (VOH) is referenced to REG1.
Is it possible to supply REG1 with 3.3 V so that the SPI interface operates at 3.3 V logic levels?