Tool/software:
Dear Mike O'
Your Suggestion given in " RE: UCC28600: 2nd and 3rd Step is not understanding "
looking wrong as per my below details.
- When you change Vout and Pout for Vout2, Vout3 … Vout7 in the tool, it also changes Pin, I_PK,pri, and L_p. That behavior is fine for a single-output design, but it’s not the right way to extract per-rail currents in a multi-output flyback. In a real converter, the primary peak current and primary inductance are set once from the total output power (sum of all rails plus losses) at the worst case.
- Each secondary then “sees” that same primary peak current through its turns ratio. So per-rail calculations must not re-optimize the primary each time you edit one rail’s power.
Below is the relation B/W Ipk_pri and Ipk_sec.
(Ip=Ipk)