Other Parts Discussed in Thread: TPS3762-Q1, TPS37100-Q1, TPS3760-Q1, TPS3700
Tool/software:
Hi
I have some questions which I was not able to answer with the datasheet.
In the datasheet, there is a latched WDO mentioned in context with WDO_DLY. How is it possible to configure a latched WDO? In our setup, WDO should be latching and stay low when the watchdog triggered.
There seems to be a mistake in the datasheet. In 7.5.1.2, register VMON_CTL, FORCE_WDO_LOW is using bit4 to bit7 but later, bit5 to bit7 are defined as reserved. Is one of the additional bits used for the latching option?
What happens when WDE changes from high->low. Will this disable the watchdog and deassert WDO? Will a following low->high restart the watchdog? Would this be comparable to write a 1 into WDT_ERROR?
There seems to be a typo in the datasheet:
"both NRST and NRST" seems to be wrong, I assume "NRST and NIRQ" is meant.
For the MONx pins, there is a maximum voltage specified. What happens, when in case of a defect of a voltage regulator, the voltage at MONx is higher? Are there clamping diodes?
Is it allowed to insert a series resistor to limit the current into the pin? When yes, what is the maximum allowed current into the pin? What type of circuit do you recommend for OV protection?
Thank you very much.