TPLD1201: DC load board total solution

Part Number: TPLD1201

Tool/software:

Dear TI Experts,

Do you have DC load board EVB total solution? what spec do you design on it? Thanks.

  • Hi Juin,

    To support these devices we use a 2 board evaluation method. 1 is a programmer (TPLD-PROGRAM) which can be used for any TPLD device, and the second is a device and package specific EVM (IE TPLD1201-RWB-EVM) This system powers the device from the USB port of the computer to do evaluation on it. The main spec we design for this board to handle is 3.3V however if the programmer is disconnected from the EVM board it is capable of handling all levels of VCC the device can handle as listed in it's datasheet.

    Regards,

    Owen