BQ34Z100-R2: GPC Tool Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data.

Part Number: BQ34Z100-R2

Tool/software:

Just trying to understand what causes this error, as my graph isn't showing anything obviously anomalous! See attached for my test data, and resultant report. I note, after performing this test and capturing all the data, that I actually need to capture the charge profile as well. Can you confirm this is required? If so, I will update my test setup and likely switch to using my BQ34Z100-R2 to capture the voltage/current/temperature instead of my test equipment.

The resultant CHEMID seems to have a 10% error - but I'm not sure if that is good enough or not. Please advise :)

encore 18650-2S16P.zip

encore 18650-2S16P-report.zip