This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: maximum load capacity in TPS55288

Part Number: TPS55288


Tool/software:

If there are specifications for the maximum load capacity in TPS55288, please let me know.

  • Hi sir,

    The expert is OoO today, please expect a delay response next Monday.

    BRs, 

    Bryce

  • Hi Sir,

    Thank you for reaching out. 

    From spec side, with 20kohm Rlim, TPS55288 has 14A minimum average inductor current limit.

    When TPS55288 works in buck/buck-boost mode, Iout equals average inductor current, then Maximum Iout equals 14A.

    When TPS55288 works in boost mode, Iin equals average inductor current, then Maximum Iout equals 14*Vin*eff/Vout.

    From thermal performance side, with Pout>60W, layout should be paid more attention and recommend to use 200kHz fsw. With Pout>100W, external thermal dissipation solution is needed.

    Regards,

    Mulin