Other Parts Discussed in Thread: BQ79616
Tool/software:
Hello, I am trying to use the BQ79616 in a supercapacitor scenario.I have 2 questions.
(1) After using an external independent power supply, we found that when the supercapacitor voltage is close to 0V or very low, the value fed back by the BQ79616 jumps, especially the third channel, which always shows a unique value. What is the reason for this? Do the sampling values of the BQ79616 fluctuate at low voltages?What should I do to ensure that the sampling values of all voltage channels are accurate at 0V?
(2) When no external power supply is used, the BQ79616 loses power due to instantaneous discharge of overcapacitance. After recharging and restarting, the BQ9616 will have abnormal power rails such as TSREF and report a fault TSREF_OSC & TSREF_UV .How do I solve this problem? Is there any way to reset BQ79616 under abnormal circumstances?