This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS923655: Information on power dissipation

Part Number: TPS923655


Tool/software:

Hello,
I try to find some information about the calculation of power dissipation of the IC for different operation conditions. I tried the preliminarry Excel calculation tool and there for my operation conditions I will get a value of more than 3W for IC dissipation and a dT of 130°C.

I entered the following values: Input voltage 48V, Output voltage 63V, LED-current 4A

switching frequency would be 400kHz.

There are no information on power looses inside the IC - so DC looses can be calculated regarding 150mOhm Mosfets, and voltage regulator is mentioned with 10mA current. For switching looses there are no informations, but in any case I will not come to more than 3W.


2. question:

To reduce the power dissipation I could supply the IC only with 12V for controlling - the LED power path needs to rund with 48V. This means, that Vin would be 12V, while SW-pin will come to 48V. Also the measureing pins for current will have a common mode of 48V.

Is this a problem and are there any points I have to take care on.

Many thanks
Juergen