Tool/software:
Hi all,
I would like to know the behavior of VS (20-23pin) when the power supply is OFF (0 V).
From "7.3.7.3 Protection against loss of power" in the data sheet,
I understand that the output is shut down regardless of the input level of IN1-4 (3-6pin).
Regarding the other input pins (SEH: 7pin, SEL: 8pin, DIAG_EN: 14pin) Behavior under the same conditions is not specified in the data sheet.
These pins are the same as IN1-4, is it correct to understand that there is no problem in operation even if a High or Low is input under the condition that the power is not turned on?
Best regards,
Ryusuke