This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: maximum Current into ESD pin protection

Part Number: BQ76952
Other Parts Discussed in Thread: STRIKE

Tool/software:

Hi,

quick question regarding the absolute maximum ratings of the Alert, shutdown and I2C pins of the BQ76952:

The Datasheet states the maximum voltage is 6,0V due to the ESD protection. However, during assembly when the connectors are plugged in, we can have some current injected into these pins. I can not find any information, how much current these pins can handle while limiting the Voltage. Normally the absolute maximum ratings should gibe a Voltage range AND a maximum allowable current rating. 

best regards,

Michael