Tool/software:
Dear,
We have some TPS2042 which fail after a while we think there are two type of fails:
1. We use one USB in OTG mode which is connected to a TPS2042 output.
What could happen is that the enable pin of the TPS2042 is HIGH (so output disabled) but there is still +5V on the output pin.
I can't really find in the datasheet if this is allowed so it could be expected that this breaks the TPS2042.
This only could happen when we are developing and not in the real product.
2. We have seen now on 2 board (of the 30 pieces which we have produced now) that the output isn't enabled when the enable pin is pulled LOW.
There hasn't been any load on the +5V (and also no other +5V applied to it). Except an LED and a 18k resistor for faster depletion of the output capacitor.
See the part of the schematic for the output:
And the input part: