Tool/software:
1.Part number:BQ24610
2.Software/Tools/models used: buck converter
3.Is the problem related to the schematic or layout?
If yes, please provide the schematic/layout:
4.Question: The input voltage is 19 V, the output voltage is 14.3 V, and the output voltage will periodically drop to about 9.8 V under no-load. The HS tube has no driving waveform periodically. Is this due to the battery detection mechanism of BQ24610 ? After adding a constant current load source at the output end, the phenomenon still exists. Is this due to the fact that the constant current load source cannot simulate the battery ? Whether it is detected as the battery does not exist, the output voltage periodically falls under the VLOWV.
output voltage waveform:
BUCK high-side tube waveform: