LM76003: Advices & quick Schematic review for a first EMC/EMI oriented design project

Part Number: LM76003
Other Parts Discussed in Thread: DRV8821

Tool/software:

Hello everyone,

I am planning to use two LM76003 as DC/DC converter on the power stage of the board I am designing right now and Iwould like to know if you could give me EMI/EMC filtering oriented advice on my powerstage design please. I'll join a simple schematic of this power stage that I'll complete with some explanations here !

First of all I am looking forward to pass the IEC-61326 standard with this board. 

concerning the following schematic:

- The +36Vdc power line is delivered by a Meanwell RSP-400-36 which is a medical field EMI/EMC designed power supply.

- The load on the +24Vdc out will be two or three stepper motors driven by two DRV8821 from TI.

- The +Vdc output will supply the logic and control electronic such as a PIC microcontroller, an RS485 transceiver or an USB module from FTDI.

Thank you in advance for your time,and your answers,

Paul.