Tool/software:
Hi i am using Tusb546A I want to know how to write the register values for example in data sheet having 8 registers in what register what data need to write for eg : flip, 4 lane dp, 2 lane dp
These are the registers from the tusb546A data sheet
1.General Register (address = 0x0A) [reset = 00000001]
2.DisplayPort Control/Status Registers (address = 0x10) [reset = 00000000]
3.DisplayPort Control/Status Registers (address = 0x11) [reset = 00000000]
4.DisplayPort Control/Status Registers (address = 0x12) [reset = 00000000]
5.DisplayPort Control/Status Registers (address = 0x13) [reset = 00000000]
6.USB3.1 Control/Status Registers (address = 0x20) [reset = 00000000]
7.USB3.1 Control/Status Registers (address = 0x21) [reset = 00000000]
8.USB3.1 Control/Status Registers (address = 0x22) [reset = 00000100]
questions
1.From the above registers we want to write each register or only 0x0A general register? give example
2. If we use general register only then all the remaining registers are write into the 0x0A ? give example code for writing through i2c
3. How to write the data in registers for dissplay lane , flip 2 ane 4 lane display lane with flip, and aux flip ?
4. for example i2c write( tusb546a slave address , register address(0x0A), register data(0x02)) is ths correct ? or i need to write only the 0x0A register address with the remaining registers as data for 0x0A ?like
i2c write( tusb546a slave address , register address(0x0A), register data(0x10))
i2c write( tusb546a slave address , register address(0x0A), register data(0x11))
i2c write( tusb546a slave address , register address(0x0A), register data(0x12))
i2c write( tusb546a slave address , register address(0x0A), register data(0x13))
i2c write( tusb546a slave address , register address(0x0A), register data(0x20))
i2c write( tusb546a slave address , register address(0x0A), register data(0x21))
i2c write( tusb546a slave address , register address(0x0A), register data(0x22))
how to i need to write the register only 0x0A or all register ?