TPS92380: Question about SW terminal behavior just after powered on.

Part Number: TPS92380
Other Parts Discussed in Thread: TPS92360

Tool/software:

Hello guys,

One of my customers is evaluating TPS92380 using the SEPIC circuit shown on page 28, Figure 9-4 of the datasheet.
At this moment, they have the following questions.
Could you please give me your reply?

Q1.
Due to the microcontroller's initial setting, VDDIO/EN, SYNC connected to VDDIO/EN, and PWM terminals are high level
for approximately 5 ms just after powered on. After that, VDDIO/EN, SYNC, and PWM terminals went to low.

Approximately 60 ms later additionally, the SW terminal cycles on and off multiple times and goes low level after that.
At this timing, the voltage at VOUT (the cathode side of the rectifier diode) is boosted.

Is this SW terminal on/off cycling normal behavior for the TPS92380?
In other words, once soft start begins, will SW cycle on and off multiple times at the end of soft start even if VDDIO/EN terminal is set low during soft start?

Q2.
When the timing that SW is turned on and off multiple times, does SW OVP and output OVP protection work correctly though VDDIO/EN = L?
If the the answer is No, is there a possibility that damaging the TPS92380 by the SW terminal voltage and output voltage rising?

Q3.
Can the information and formulas in 8.3.1.2.1 "Using Two-Divider" and 8.3.1.2.2 "Using T-Divider" be applied to SEPIC mode?

Q4.
Is the content of 9.2.3.1 "Inductor Selection" applicable in SEPIC mode?
It also states that "A saturation current rating of at least 4.1 A is recommended for most applications.."
However, the TPS92380's maximum current IMAX is 120mA, which is far more than 4.1A.
What is concern when the inductor saturation current is less than 4.1A and why is it set at 4.1A?

Your reply would be much appreciated.

Best regards,
Kazuya.