Other Parts Discussed in Thread: BQ29209
Tool/software:
Hi, TI E2E
I want to design a Li-Ion battery, but I'm uncertain if the design need to do any more modify?
The design need to do the IEC-62133 verification.
The design is refer from each component datasheet or EVB.
0.Li ion use: Samsung INR18650-35E, 2 Series 3 Parallel, 0.5C (max charging current<4.95A)
1.battery balance and protect IC use: BQ29209DRBR,
2.battery charger IC use: BQ24171RGYR
In this design set as 4A, could modify the output L and C to config the charging current
3.buck IC use: TPS566247DRLR (6A)
The total current from the load(SBC,FAN,HMD) is 5A(peak), could I just use one of this buck?
Thank you
Best Regard Steve