Tool/software:
Hi Team,
I am digging into the RESET delay time accuracy for the TPS3808 when I came across another thread listing the breakdown of how the 40% accuracy variance is calculated.
E2E - TPS3808: True Accuracy of TPS3808
According to Jesse, the 40% accuracy variance includes an assumption of a 20% tolerance capacitor, yet this 40% accuracy variance remains the same even when removing the capacitor from the equation. Can you provide any guidance as to why this is or how much of an impact does the Ct capacitor truly make on the reset delay time?
Regards,
Filipe Rubinstein