Other Parts Discussed in Thread: REF34-Q1
Tool/software:
I am using REF3450 for an automotive application. I have a question if the input voltage goes below 5V, what would happen to the output voltage.
Hi Abba,
The REF34-Q1 has a dropout voltage relative to the load current drawn. At its highest the dropout voltage is 500mV. In the case where the voltage goes below this needed Reference voltage + droput = 5V + 0.5V = 5.5V, the output voltage will drop with the input voltage as input voltage minus dropout voltage.
Thanks,
Joshua