TPS65982: Migrate to TI new USB-C PD chips

Part Number: TPS65982
Other Parts Discussed in Thread: TPS26750, TPS25751

Tool/software:

Hi Team,

We have a USB-C hub that uses the TPS65982 to charge an upstream notebook PC and provide 4 downstream ports. In this design, the TPS65982 acts as a source and provides 5 V / 12 V / 15 V / 20 V by switching the feedback resistors of a buck converter through its GPIO pins. It also controls the USB SuperSpeed MUX via a GPIO. These GPIO functions can be configured using the customization tool.

Could you recommend TI devices such as the TPS26750 for a similar application? From what I have seen, the web-based customization tool does not provide options to configure GPIO pins, and I am also unable to download a Windows offline version.

Steve