UCC28083: Request for schematic design review

Part Number: UCC28083

Tool/software:

Hi Team,

There is an issue that UCC28083 is not started up on the customer board. Their board specifications are as follows. And VDD pin voltage is measured to 12.5V, and current is measured to 0mA. Please check the schematic below and let me know the review result.

1. Start up current : 120uA to 200uA

2. Supply current : 1.5mA to 2.5mA

3. Start threshold voltage : 11.5V to 13.5V

Schematic_UCC28083.pdf

Regards,