Tool/software:
Hi there,
I use the LM 3150 to step down from 26V to 21.3 .
Input should be max. 2.3 A.
Its to charge a LiFePO Battery.
When i connect first the input at 26 V then the Battery its working.
If the Battery is connected first it will destroy the controller evry second or thirt time.
Can you help me to save the chip?
Its very urgent.
Thank you
Ingo