Tool/software:
Hello team,
I could not understand how to set PD negotiation from the TPS25763-Q1 data sheet, how do I switch between normal USB mode and DP Alternate mode?
[PD Negotiation]
Can the TPS25763-Q1 negotiate PD with device connected via USB?
And is the negotiation configurable in I2C?
[Entry trigger to DP Alternate mode]
When the TPS25763-Q1 is operating as a power source and normal USB DFP, can it send command to enter DP ALT mode at any time?
[Exit trigger from DP Alternate mode]
When the TPS25763-Q1 is operating as Power Source and DisplayPort Sink, can it send command to exit DP Alternate mode at any time?
Or it can only do by DisplayPort Source side?
Regards,
Youhei MIYAOKA