Tool/software:
Hello, for my application there will almost always be a source connected to the Vin pin of the BQ25185 charger. I don't want it always trying to charge my secondary battery as soon as the voltage drops below its max voltage. Is there any wiggle room to get a resistor value that will get a VBATREG not listed on this table shown in the datasheet? For clarity, my battery has a max voltage of 4.1V. I would prefer not to have the charger always trying to charge it to 4.1V. Instead, I would like to charge to a voltage like 3.9V that way my battery can sit without being charged as often. My application has this charger acting standalone so there would not be a microcontroller that could control the /CE pin.
Any help would be appreciated. Thank you!