This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74680: OUTP

Part Number: LM74680

Tool/software:

Hi All

I have a question about the LM74680.

If a PFC circuit is placed after the LM74680, I think that when the input voltage drops, the voltage at the LM74680's OUTP and EN terminals will also drop.

For example, when the input voltage is 24vrms/50Hz, I think that there will be times when the LM74680's OUTP is insufficient while the input voltage transitions from 0V to 5V and from 5V to 0V (equivalent to 0.5ms x 2, 10% dead time). Will this pose a problem for the LM74680?

Also, will there be any problems with the LM74680 if OUTP fluctuates?

Best Regards,
Ishiwata