Hi,
I am currently using the LM5069 part in one of the power supply application,in which I am switching the 40V from a DC-DC Converter to the output load.Now I am facing a issue of Mosfet failure in two conditions.
There are two power supply boards:
1). 40V,5A Current limit was set to 5.25A
2).40V,18A, Current limit was set to 19A
i). When I add a capacitive load at the output of the controller and mosfet source, the mosfet was failed due to the inrush current offered by the Capacitive load of 2000uF and above, then we increased the timer Capacitor of the controller to1uF from 0.1uF in order to avoid the over-load shutdown due to inrush during the startup. Then the 40V output was coming properly. Then we increased the timer cap to 4.7uF in order to avoid OL- shutdown with 4000uF capacitance. Now the board is working in 5A current application.
The DC-DC Converter used in the board has an inbuilt short circuit protection (Hiccup mode), when we checked for the short circuit test by shorting the Mosfet source to ground the Mosfet failed again. We suspect the problem could be due to the Safe operating area of the mosfet.
Hotswap part number : LM5069mm-1
Mosfet part number : SI7174DP-T1-GE3
The similar problem exists in other 40V,18A board . So request you to help on the same.
Thanks in advance,
Vinoth