Tool/software:
Hi Teams,
At present, the customer's actual measured output current with load cannot reach 4A. Please help to investigate the possible reasons and provide any good suggestions. Thank you~5125.IRLED-0725.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Teams,
At present, the customer's actual measured output current with load cannot reach 4A. Please help to investigate the possible reasons and provide any good suggestions. Thank you~5125.IRLED-0725.pdf
Dear Sir,
Pls try below suggestions and see if there is any improvement.
(1) Change R5 to 0ohm;
(2) Change R3 to 100ohm;
(3) Change C18 to 1nF;
(4) Re-design R6 and R7 according to
Hi Lucia,
The customer tried the suggestion you provided, but still couldn't reach 4A, at most around 3A. The current setting for the sampling resistor is 50 milliohms for the customer
Corresponding to 4A, R6, and R7, they can be completely suspended without the need for low voltage detection. Do you have any good suggestions?
翻译
搜索
复制
Hi Vayne,
I am not sure if customer has adjusted UVP resistors. Just like the FAQ I shared, To make sure your output current won't be affected in all working condition, you should make sure (Vin_min - Vout_max) * R_UVP2 / (R_UVP1 + R_UVP2) > 1.4V.
For example, input voltage range: 9-12.6V
(9-7.2)*102/411k=0.45<1.4V. Besides, A rule of thumb is that you can design the sum of R_UVP1 and R_UVP2 to be around 1Mohm or 2Mohm and this normally would be a good start point.
Thank you!
BRs
Lucia