This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5891-Q1: Control method if 2 LP5891-Q1s are used

Part Number: LP5891-Q1
Other Parts Discussed in Thread: LP5899

Tool/software:

Dear TI experts,

My customer now checks the specification of LP5891-Q1 for their next project.

They already tested one LP5891-Q1 with F280039C which is referenced in EVM user's guide.

But they want to use (LP5891-Q1 x 3) x 2, total 6 LED drivers.

I already know that LP5891-Q1x3 can control using only 1 MCU, but if I should control another LP5891-Q1x3 drivers, should I use 1 more MCU to control separately?

Or it is okay to use 1 MCU to control these 2 modules?

And one more question - If I have use 2 MCUs, Is there any considerations like synchronization or other point of view?

Please check this issue. Thanks.

Best regards,

Chase